Tokyo, Japan, June 22, 2012 — NSK Ltd. (NSK; Headquarters: Tokyo, Japan; President and CEO: Norio Otsuka) announced today that it will be exhibiting at the 25th INTERPHEX JAPAN from Wednesday June 27 to Friday June 29 at Tokyo Big Sight. INTERPHEX JAPAN is a large-scale trade show in Asia with devices, systems and technologies related to the production, research and development of items such as medicine, cosmetics and detergents. NSK will be exhibiting its state-of-the-art products and technologies that provide solutions to the diverse and advanced needs of these industries, which require a high-level of safety.
NSK has put together a variety of solutions for ensuring the high-level of safety required in the backbone components used to support the stable operation of production equipment used in fields such as medicine, cosmetics and detergents that assist consumers in achieving their ultimate desire to be healthier and more beautiful.
This is the fourth time for NSK to participate in this exhibition, and this year the theme will be Oil Splashing and Corrosion — That Is the Problem. NSK will showcase its highly practical applications comprised of its proprietary technology and products that incorporate oil splashing countermeasure technology and corrosion resistance that is more than 10 times better* than conventional technology. NSK will also exhibit its highly clean and compact mechatronics technology for those on the frontlines of the manufacture, research and development of medical and cosmetic products.
| *Note: | In terms of the time it takes for rust to occur during immersion testing using sodium hypochlorite, a sanitizing and disinfecting agent. |
SUS Barrier™ Bearings