MEGATORQUE MOTOR SETUP for EGC Application Download

About MEGATORQUE MOTOR SETUP for EGC Application

Description of Operation

This application can communicate with the Driver Model EGC from a PC to rewrite and save various parameters and perform JOG operation.

1. Setting of general parameters such as position, speed loop proportional gain, etc.

2. Setting of Driver Model EGC system parameters.

3. Monitoring the status of the Driver Model EGC connected to a PC via cable

4. JOG operation by speed.

5. Operation trace function and system analysis function.

This application is provided free of charge upon acceptance of the terms and conditions of use.

MEGATORQUE MOTOR SETUP for EGC Application Operation Environment:

PCIBM PC/AT-compatible
MemorySpace more than 512MB
Hard-disc spaceMore than 1GB (Including Microsoft .NET Framework 3.5)
DisplayMore than 1024 x 768 of resolution/ 32 color-bit
Applicable OS

WIndows® 10
WIndows® 11
Note) There is no limit to the edition of operating software.

Requird software

The following components are required to operate this application. If they have not been installed berfore installing this application, they will be automatically installed.

  • Microsoft .NET Framework 3.5
  • Crystal Reports Basic Runtime for Visual Studio 2008
  • TDM-GCC
  • MATLAB Runtime 9.0
OthersOne or more USB ports
Installing MEGATORQUE MOTOR SETUP for EGC Appliation

You can install this application by launching the EXE file after unzipping the downloaded ZIP file.

Follow the installer's instructions to complete the installation.

How to Use MEGATORQUE MOTOR SETUP for EGC Application

After installation completes, please see “Help.”

Notes:

  1. Company and product names listed are registered trademarks of their respective companies.
  2. The reproduction, copy, or alteration of information contained within without permission from NSK Ltd. is prohibited.
  3. The information contained within is subject to change without advance notice.

NSK Program License Agreement

This “Program” is copyrighted by NSK Ltd. (hereinafter NSK) and is not for sale; it is licensed for use. Under the terms of this License Agreement, NSK grants the user usage rights to the “Program” in the country where downloaded (hereinafter the “Usage Agreement”). NSK assumes no responsibility for the installation, usage, or results of the “Program” or that these will meet user expectations.

1. Usage Rights

Use of the “Program”

For each download of the “Program”, the user may (1) use the “Program” on one machine, or (2) transfer the “Program” to a third party.

If the “Program” is transferred to a third party, this “NSK Program License Agreement” must also be transferred. The user may transfer the program to a third party provided that the transferee agrees to the “NSK Program License Agreement.” Once a third party has agreed to the agreement, the original user’s usage rights will end.

The user must NOT (1) transfer or use the “Program” in any way not specified by this License Agreement; (2) transmit the “Program” by e-mail, etc.; (3) duplicate, change, combine, or distribute the “Program”; (4) decompile, disassemble, reverse engineer, or adapt the “Program”; or (5) relicense, lease, or loan the “Program.”

2. Copyright

In all cases, the copyright for this software, documentation, etc. belongs to NSK.

3. Warranty

This program is provided as is with no warranty of any kind.
No program services such as upgrades, etc. will be provided.
The warranty specified above for the “Program” is in lieu of all other warranties, express or implied, and including those statutory warranties against defects, for merchantability, or of fitness for purpose.

4. Limitation of Liability

NSK is not liable for lost profits, indirect damages, extended damages, or damages that occur for extraordinary reasons, either foreseen or unforeseen.
NSK is not liable for claims for damage from a third party. The above Limitation of Liability also applies to claims for damage/loss against the “Program” developer who supplied the “Program” to NSK.

5. Other

The user may terminate this Usage Agreement at any time without notifying NSK. In this case, the user’s usage rights for the “Program” will be terminated.
NSK may also terminate this contract if the user violates this Usage Agreement. In this case, the usage rights for the program will be revoked, and the user must delete, destroy, or otherwise make unusable any copies of the software they possess.

MEGATORQUE MOTOR SETUP for EGC Application Download

Please download the appropriate file below and install the application.

CategoryNameFile TypeFile
Size
Ver.
(Release Date)
SoftwareMEGATORQUE MOTOR SETUP for EGCZIP389 MB
V001-000-001-002-000-000
(2025/08/29)