NSK will exhibit at IPF Japan 2023 (International Plastics Fair) to be held at Makuhari Messe (Chiba City) from November 28 to December 2, 2023.
Global
ASEAN and Oceania
Middle East
Africa
Press Release
November 22, 2023
NSK Ltd.
Corporate Communications Department
NSK will exhibit at IPF Japan 2023 (International Plastics Fair) to be held at Makuhari Messe (Chiba City) from November 28 to December 2, 2023.
We will showcase high-performance products and services that harness NSK's technological expertise. Additionally, we will propose solutions to address diverse needs in the production field and societal demands such as environmental impact reduction, taking manufacturing to the next level.
Achieves a permissible d·n value of 200,000 and a transient maximum temperature of 100°C through the newly developed SRM ball recirculation and heat-resistant components. Contributes to further reduction in cycle time for injection molding machines.
We developed a technology that up to doubles ball screw life (compared to conventional products) by optimizing the load balancing in each recirculation circuit. Longer life contributes to improved productivity and resource conservation in industrial machinery. The applicable product range has been expanded from 4 to 19 models.
Ideal even for customers considering implementing predictive maintenance strategies for the first time. With no need for wiring work as long as there is a wireless internet network, the system can perform condition monitoring from the cloud. Utilizing proprietary diagnostic indicators and AI, it enables the early detection of equipment abnormalities. Furthermore, diagnostic specialists can remotely analyze the data and propose solutions and maintenance measures.
High-accuracy onsite method to rapidly diagnosis the remaining life of lubricant grease; simply sample a small amount of grease. By quantitatively evaluating the color change of the grease using a mobile app, the remaining lifespan of the grease can be diagnosed. The high-accuracy analysis of grease using the mobile app alone is a world-first.
| Exhibition | IPF Japan 2023 |
|---|---|
| Venue | Makuhari Messe (Chiba) |
| Dates | November 28 to December 2, 2023 |
| NSK Booth | Hall 3, 31307 |
| Official website | https://www.ipfjapan.jp/english/
|