NSK Ltd. (NSK; Headquarters: Tokyo, Japan; President and CEO: Toshihiro Uchiyama) today announced that it has expanded the size of its NSKTAC03 high-load drive ball screw support bearings for large electric injection molding machines. NSK is targeting 1 billion yen in annual global sales for this product series in 2018.
As automobiles become more energy efficient and emission regulations become even stricter, there is a greater need to reduce the weight of hybrids and electric vehicles. This need is in turn driving the need for larger plastic components such as large one-piece bumpers and door modules, as well as instrument panel interior components.
In the past, hydraulic injection machines capable of high loads were the solution for forming these large components. Today, however, electronic injection machines, which are energy efficient and clean (since they do not require oil), are seeing greater and greater demand.
- 1. Product Benefits
- Compared to thrust self-aligning roller bearings, which have been broadly used to date, this newer product uses half the torque and rotates smoothly in both forward and reverse directions.
- 2. Hanging bolt holes come standard
- Hanging bolt holes are now standard, so it is easy to use cranes to assemble heavy bearings. This helps to improve efficiency at production sites.
The increasing size of electric injection molding machines and servoless machines has heightened demand for drive ball screws with a higher capacity. As such, the need for higher performance in support bearings has also increased. In 1996, NSK launched its dedicated support bearing for high-load drive ball screws. Since then, NSK has continued to expand its product lineup for higher loads and other special needs. NSK is committed to providing solutions as Your Real Partner.™ by continuing to meet various market needs.