NSK Ltd.
CSR Division Headquarters
Public Relations Department
NSK Develops Ultra High-Speed Large-Diameter Ball Bearings for Motors in Hybrid Cars
Bearings help to improve fuel economy and raise power output
Tokyo, Japan, July 5, 2011 – NSK Ltd. (NSK; Headquarters: Tokyo, Japan; President and CEO: Norio Otsuka) today announced that it has developed large-diameter bearings for motors that are capable of ultra high-speed rotation exceeding two million dmn*1. The new products deliver the fastest*2 rotation speeds of any other ball bearing used for automotive applications, and can be utilized in ultra high-speed motors to help improve fuel economy and driving performance. NSK is targeting annual net sales of ¥3.5 billion of the products by 2015.
*1 dmn: Bearing diameter × Maximum rotating speed
*2 According to our own research, as of July 2011
There is an increasing diversity of hybrid systems aimed at delivering better fuel efficiency and higher motor power output for driving. For hybrid car motors, there is increasing demand for larger diameter bearings, as motors increase in size and with the development of ultra high-speed motors that deliver higher power output.
The large-diameter ball bearings for hybrid car motors have an inner diameter of 160 mm and outer diameter of 190 mm, yet in spite of their size are capable of ultra high-speed rotation exceeding two million dmn, faster than any other ball bearing used for automotive applications.
The new ball bearings will help to improve the fuel efficiency and driving performance of hybrid cars, by enabling drive motors and generators that enhance power output and fuel efficiency in hybrid cars.
Product features
The superior features of this product, as detailed below, enable it to deliver ultra high-speed rotation.
◆Carbon fiber reinforced PEEK cage
To deal with the tremendous centrifugal force generated by the high-speed rotation of large-diameter bearings, carbon fiber reinforced PEEK is being used for the first time ever as a cage material for automotive bearings, dramatically improving cage durability.
◆Inner ring guide
The use of a crown cage for the ball guide along with the outer diameter of the inner ring as guide surfaces controls vibration and skidding damage resulting from cage runout, dramatically improving bearing durability during super high-speed rotation.
◆Optimized internal design and long life technology
Optimized radial clearance, ball diameter, number of balls, and groove dimensions inside the bearing module control friction and heat generation even under ultra high-speed rotation, preventing seizure. In addition, the use of heat treatment technology and a material with superior dimensional stability on the inner and outer rings controls age deterioration of dimensions and radial clearance during usage, improving durability.
Product Features
A technological breakthrough enabling super high speeds
Bearing size:
Inner diameter: Up to φ160
Outer diameter: Up to φ190
Product Features
The superior features of this product, as detailed below, enable it to deliver ultra high-speed rotation with a dmn value of 2 million that is unmatched anywhere in the world for use in automotive applications, while maintaining ultra large-diameter bearings with an inner diameter up to φ160 and an outer diameter up to φ190.
1. Carbon fiber reinforced PEEK cage
To deal with the tremendous centrifugal force generated by the high-speed rotation of large-diameter bearings, carbon fiber reinforced PEEK is being used for the first time ever as a cage material for automotive bearings, dramatically improving cage durability.
2. Inner ring guide
The use of a crown cage for the ball guide along with the outer diameter of the inner ring as guide surfaces controls vibration and skidding damage resulting from cage runout, dramatically improving bearing durability during super high-speed rotation.
3. Optimized internal design and long life technology
Optimized radial clearance, ball diameter, number of balls, and groove dimensions inside the bearing module control friction and heat generation even under ultra high-speed rotation, preventing seizure. In addition, the use of heat treatment technology and a material with superior dimensional stability on the inner and outer rings controls age deterioration of dimensions and radial clearance during usage, improving durability.
Evaluation Result
Test condition
Load
unloaded (only imbalance load due to rotational load)
Rotation speed of outer ring
10,080 rpm
Rotation speed of inner ring
4,255 rpm
* dmn
2.6 million equivalent (converted to cage orbital speed)