Tokyo, Japan, December 19, 2011 – NSK Ltd. (NSK; Headquarters: Tokyo, Japan; President and CEO: Norio Otsuka) today announced that it has developed a low-torque tappet roller bearing for automobile engines. Through the use of special heat treatment, the new bearing achieves extended life and increased capacity in a more compact, lighter solution. NSK aims to contribute to improved fuel economy with this product and is targeting 1.5 billion yen in sales in 2016.
In recent years, as environmental awareness has increased, the demand for greater fuel economy in cars has risen, which has resulted in the need for improving fuel economy in engines by means such as reducing size, weight and torque loss. This, in turn, has resulted in the pursuit of an even greater level of efficiency as developers sought to improve peripheral engine parts and introduce a variable valve timing mechanism. This product contributes to higher engine efficiency through the following superior features.