Tokyo, Japan, April 14, 2010 - NSK Ltd. (NSK; Headquarters: Tokyo, Japan; President and CEO: Norio Otsuka) announced today that it has developed a more compact, lightweight, longer-lasting lipped thrust race for use in automatic transmissions.
Global
ASEAN and Oceania
Middle East
Africa
Press Release
April 27, 2010
NSK Ltd.
CSR Division Headquarters
Public Relations Department
Helps Make Automobile Transmissions More Compact, Lightweight, and Efficient
Tokyo, Japan, April 14, 2010 - NSK Ltd. (NSK; Headquarters: Tokyo, Japan; President and CEO: Norio Otsuka) announced today that it has developed a more compact, lightweight, longer-lasting lipped thrust race for use in automatic transmissions.
Low viscosity transmission oil is commonly used today to improve transmission efficiency, but this creates lubrication challenges. NSK's new product is designed for outstanding performance in severe lubrication conditions, and also helps to improve fuel economy. NSK expects sales of this product to reach one billion yen by 2015.
In recent years, automakers looking to improve fuel economy, reduce gear shift shock, and raise power transmission efficiency have increasingly turned to multi-stage automatic transmissions. Low viscosity transmission oil is often employed in these transmissions to reduce agitation resistance, which has a negative impact on transmission efficiency. This type of oil presents lubrication challenges for the thrust needle bearings typically used in transmissions. Meanwhile, demand is on the up for more compact, lightweight transmission bearings that can help improve fuel economy in hybrid electric vehicles (HEVs). But when HEVs run on the electric motor alone, the oil pump sometimes stops, which in turn means that the thrust needle bearings in the transmission have to function on lean lubrication. NSK's new lipped thrust race will help improve fuel economy and reduce CO2 emissions by meeting the need for more compact and lightweight bearings that are more than ready for challenging automotive applications. Product features are summarized below.