Tokyo, Japan, September 29, 2009 – NSK Ltd. (NSK; Headquarters: Tokyo, Japan; President and CEO: Norio Otsuka) has developed new cages and rollers for planetary gear mechanisms (hereinafter referred to as “planetary gears”) for use as cages and rollers for miniature planetary gears with high-speed rotation specifications. NSK expects annual sales to reach 2.5 billion yen by 2015 given that these products meet the need for miniaturized, lighter-weight, higher-output belt CVTs, ATs, and hybrid vehicle transmissions.
In recent years, an increasing number of ATs have employed multistage gears for up to eight speeds within a compact space to mitigate shocks caused by gear changes and improve the power transmission efficiency to achieve a reduction in CO2 emissions and higher fuel economy In addition, high-speed rotation that can generate higher output with smaller motors for hybrid vehicles is being developed. Given this, there is demand for not only high-speed rotation, but also a reduction in the size and weight of the cages and rollers used in planetary gears to change gear speeds and transmit the torque in transmissions. NSK is contributing to improved fuel efficiency in vehicles and thereby reducing CO2 emissions and improving the efficiency of gear speed changes by developing these products with the following features.
Features of cages and rollers for miniature planetary gears.