Press Release
Search suggestions

NSK Welcomes Visitors to SEMICON Japan 2015

Technology and Products That Support Development of State-of-the-art, Next-Generation Devices

SEMICON Japan logo

NSK Ltd. (NSK; Headquarters: Tokyo, Japan; President and CEO: Toshihiro Uchiyama) today announced that it will exhibit its products and technologies at SEMICON Japan 2015, to be held at Tokyo Big Sight (Koto-ku, Tokyo) from Wednesday, December 16 to Friday, December 18.

Driven by the immense demand for smartphone and automobile applications, the semiconductor market is expected to maintain robust growth. Semiconductors are being pushed to offer greater performance, multifunctionality, speed, and power savings, all while being smaller, lighter and lower in cost than ever.

In response to these demands, under the theme of Your Real Partner™., NSK has put together technologies and products that will support your company's development of state-of-the-art, next-generation devices. For example, bearings that can withstand special environmental conditions such as high temperatures and corrosion, and technologies and products for super-high levels of precision guides and longer life.

In addition, NSK will show its vast lineup of standard inventory parts such as NSK Linear Guides™ and ball screws that help to reduce costs and speed up the production startup of your company's devices.

NSK's Technological Contributions

  1. Advanced clean technologies needed for miniaturization of semiconductor manufacturing processes
  2. Shorter product development and production lead times
  3. Improved maintainability and reliability
NSK booth image
NSK booth image

Main Exhibits

Dynamic Display: High-precision vertical axis table (first time on display)
Highly precise straightness reproducibility through the application of air bearings in a vertical guide
High-Performance Precision Ball Screw
Improved productivity by greatly reducing noise and vibration through optimization of the screw groove design
Megatorque Motors™ PB Series
Achievement of the industrial top-class clean level of IS03 by using Megatorgue Motors™ PB series, which have great cost performance
Dynamic Display (Reference Exhibit): Z-θ Integrated Actuator Capable of Independent Elevation and Rotation
Image of conveyance of light loads
Static Display: Special Environment Bearing SPACEA™ Series
Special bearings that can withstand high temperature and vacuum environments

*NSK will also provide videos of its exhibit on the NSK channel on YouTube starting from the first day of SEMICON JAPAN 2015

Exhibition Overview

Expo Name SEMICON JAPAN 2015
Venue Tokyo Big Sight (Koto-ku, Tokyo)
Dates 10:00-17:00, Wednesday December 16 to Friday December 18, 2015
NSK Booth location East 4 Hall, No. 4432 booth
Event URL http://www.semiconjapan.org/en/   new window

NSK makes the most of its years of expertise and outstanding technology development capabilities to continually provide customers with products that are highly reliable, deliver improved productivity and quality offer superior environmental and energy-saving performance, and keep maintenance costs low.