Tokyo, Japan, July 8, 2013 – NSK Ltd. (NSK; Headquarters: Tokyo, Japan; President and CEO: Norio Otsuka) today announced that it has developed a lubricant grease made from 100% food-grade ingredients, the first of its kind in the world. The grease is registered as an NSF*1 category H3*2 lubricant.
The grease is injected in rolling bearings that have been added to NSK's SPACEA™ Series stainless steel rolling bearings. Samples of the new rolling bearings will be exhibited for the first time at the 26th INTERPHEX JAPAN trade show for the pharmaceutical and cosmetic industry, taking place from July 10–12, 2013 at the Tokyo Big Sight venue in Koto-ku, Tokyo.
| *1: | National Sanitation Foundation (NSF) International is a not-for-profit, independent certification organization based in the United States that is recognized as an international authority in the field of public health and safety. |
| *2: | Category H3 covers lubricants intended for food contact, and are used to prevent rust on trolleys or meat hooks such as used in meat processing plants. H3 lubricants must meet the highest standards for safety, exceeding that of H1 lubricants. Category H1 covers lubricants intended for use where the lubricant may incidentally come in contact with food. |