Global
ASEAN and Oceania
Middle East
Africa
Press Release
April 28, 2009
NSK Ltd.
CSR Division Headquarters
Public Relations Department
Tokyo, Japan, April 28, 2009 – a music instrument called BEARINGS GLOCKEN II is available to rent for various events. This device is an upgraded version of BEARINGS GLOCKEN I, which was created in commemoration of NSK's 90th anniversary in 2006 with the aim of making people more familiar with bearings.
BEARINGS GLOCKEN is a musical instrument whose design is based on a new concept. A self-playing glockenspiel that was designed through collaboration between NSK and the artist Kohske Kawase, it uses steel balls made for bearings. Bearing balls, which are said to be the most perfect spheres on Earth, are rarely seen since they are usually incorporated into machines.
BEARINGS GLOCKEN II now has a repertoire of five musical works, and people will enjoy listening to its intriguing tone.
BEARINGS GLOCKEN II will be displayed at the 10th Spiral Independent Creators Festival (SICF) Grand Prix Artist Exhibition to be held at Spiral Garden, Aoyama, Tokyo, beginning Tuesday, April 28, 2009.
NSK hopes that you will attend the exhibition and take advantage of this opportunity to enjoy listening to the instrument's soft yet rich tone.
Size | 1,450mm(w)×1,400mm(d)×1,450mm(h) |
---|---|
Weight | 205kg |
Music |
|
At the exhibition, a presentation will be given to explain all there is to know about BEARINGS GLOCKEN. Covering how the first BEARINGS GLOCKEN was developed and providing an explanation of each song played by BEARINGS GLOCKEN II, this presentation will also include a demonstration video.
Name | 10th SICF Grand Prix Artist Exhibition |
---|---|
Dates | Tuesday, April 28 through Tuesday (national holiday), May 5, 2009 |
Venue | Spiral garden (Spiral 1F, 5-6-23 Minami-Aoyama, Minato-ku, Tokyo) |