Fits and Internal Clearance

Chapter 8: Fits and Internal Clearance

Bearing fit and internal clearance have a huge impact on performance. Selecting an improper fit can cause bearing damage such as creep, while an improper clearance can cause bearings to seize.

Fits

Fits define the relationship between a shaft and a hole. In bearings, this is determined by the setting of mutual dimensions and tolerances between the inner ring bore diameter and shaft diameter or between the outer ring outside diameter and housing bore diameter. Fits use tolerances to account for variations in machining and are classified into three types:

A table explaining the differences of loose (clearance), intermediate (transition), and tight (interference) fits. Loose fits always have a gap, intermediate may or may not have a gap, and tight fits always have no gap. Mounting and dismounting is more difficult for tighter fits.

Importance of Fits

Imagine an industrial motor bearing with inner ring load (a tight fit inner ring and loose fit outer ring).If the fit between the shaft and inner ring is reduced due to surface roughness, rising temperatures from operation, or high load, a clearance could develop at the fitting surface, causing fretting*, creep, or other damage. Continued use of the bearing in this state will cause additional wear at the fit surfaces, vibration, and abnormal heat generation.

*Wear from repeated relative micro-slips between two surfaces.

When a bearing is mounted on a shaft with too tight of a fit (excessive interference), stress begins to concentrate and exceed the tensile strength of the inner ring material, making it likely to crack. Even if the inner ring does not crack, lower clearance inside the bearing from expansion of the inner ring during mounting may cause abnormal heat generation. 

Always carefully consider operating conditions when choosing a fit. ​

Damage from Improper Mounting

Fretting damage on the inner ring of a bearing.

Inner ring fretting

Inner ring creep and associated scoring damage.

Inner ring creep with scoring

A cracked inner ring.

Inner ring cracks

Melting on the inner ring from component seizure.

Inner ring seizure

Creep

When a bearing is mounted on a shaft with little interference and rotates with load on the inner ring, detrimental circumferential slippage may occur between the inner ring and the shaft. ​ This harmful slippage is called creep, and it is more likely to occur when the tightness of the fit decreases. ​

If the ring is stationary in the direction of the load (inner/outer ring static load), no force that can move the ring will be generated at the fitting surface. However, if the ring rotates in the direction of load and there is a clearance at the fitting surface (or one develops), creep will occur circumferentially.

Interference is often impacted by multiple factors—Let’s look at an example of  how interference ciould decrease in a bearing with rotating inner ring load:

  1. The bearing was press-fit onto the shaft, but the shaft had some rough areas. Press-fitting causes plastic deformation at the same level as the surface roughness, so interference is reduced.
  2. When radial load is applied, the inner ring becomes compressed in the radial direction, causing slight widening and a longer circumferential length that causes a further decrease in interference.
  3. Bearing temperature rises during operation, further decreasing the interference.
かじりを伴った内輪クリープの例

Example of inner ring creep with scoring

How Creep Occurs

Animation of creep in a bearing. When a bearing is not fit properly, harmful circumferential slippage can occur between the inner ring and shaft. The inner ring is displaced ("creeps") relative to the shaft, resulting in wear and heat that can develop into significant damage.

If the interference between the inner ring and shaft is reduced and a clearance (c) develops, the circumferential length of the inner ring side (inner ring bore diameter) π (d + c) will become longer than that of the shaft side (shaft outside diameter) π d in the fitting area.


In this state, when the shaft makes one rotation, the rotation of the ring lags behind that of the shaft, as shown here.  
 

If the clearance between fitting surfaces is c, the bearing will be slowed toward the direction opposite the shaft’s rotation by πc per revolution.

Selecting a Fit

Load Conditions and Fits

Table of appropriate fits for load and rotation conditions, with example machine applications and bearing configurations.

Notes on Load Conditions

  • Rotating inner ring load: Load does not follow inner ring rotation (loaded zone on the inner ring changes)
  • Rotating outer ring load: Load does not follow outer ring rotation (loaded zone on outer ring changes
  • Stationary outer ring load: Load follows outer ring rotation (loaded zone on outer ring does not change)
  • Stationary inner ring load: Load follows inner ring rotation (loaded zone on outer ring does not change)

 

 

Shaft Fits

Tolerance ranges for shaft fits are arranged in the following order from loose to tight fits:

f, g, h, j, js, k, m, n, p, r

Diagram of tolerance for shaft fits.
Example coding for fitting tolerance of shaft/inner ring bore (Φ50k6).

1: Basic dimension

2: Shaft fit tolerance

3: IT* Class: 5 to 10
*International Tolerance: Tolerance classes specified by ISO.

Housing Bore Fits

Tolerance ranges for housing bore fits are arranged in the following order from loose to tight fits:

F, G, H, J, JS, K, M, N, P

Diagram of tolerance ranges for different types of housing fits.
Example coding for fitting tolerance of housing bore/outside diameter(Φ100H7).

1: Basic dimension

2: Housing fit tolerance range

3: IT* Class: 5 to 10
*International Tolerance: Tolerance classes specified by ISO.

Internal Clearance

Internal clearance (often simply called "clearance") is the amount of play between the inner/outer rings of a bearing and the rolling elements. More specifically, internal clearance measures how much an inner/outer ring can be displaced radially or axially relative to the other ring. ​

The amount of internal clearance greatly affects bearing performance, including fatigue life, vibration, noise, and heat generation. ​

Generally, stable measurement values for internal clearance are obtained by applying a specified measuring load to the bearing. ​

Therefore, the value for measured clearance (also called "geometric clearance" for radial bearings) is slightly larger than the theoretical internal clearance by the amount of elastic deformation (penetration depth) caused by the measuring load.

In ball bearings, we must correct for this increase caused by elastic deformation to obtain the proper theoretical internal clearance. Elastic deformation in roller bearings is minimal and can be ignored. ​

2D cross-sections of radial and axial internal clearance in a ball bearing. Radial and axial internal clearances are defined as the total amount that one ring can be displaced relative to the other in the respective direction.

How Clearance Decreases

Initial Clearance


The clearance (internal) before mounting.

 

2D cross-section of initial clearance in a ball bearing.

Residual Clearance

The clearance after mounting.
When a ring is mounted to a shaft or housing with a tight fit, clearance will decrease if the rings expand or contract.

2D cross-section of residual clearance in a ball bearing.

Effective Clearance

The clearance during operation.
Since the housing generally dissipates more heat than the shaft, a temperature difference develops between the inner and outer ring, and the resulting thermal expansion causes clearance to decrease.

2D cross-section of effective clearance in a ball bearing.

Effective Clearance and Bearing Life

Graph of the effect of clearance on bearing life. Bearing life is longest with a slight preload (negative clearance) but too much preload rapidly lowers life.

Theoretically, bearing life is longest when the effective clearance Δ of the bearing is very slightly negative. However, if excessive, bearing life decreases sharply as shown. ​

Therefore, technicians typically aim for the effective clearance to be just slightly larger than zero while accounting for the various errors unique to the actual equipment. ​

As clearance is so integral to bearing life, ISO and JIS have specified several clearance ranges.

Selecting Internal Clearance

The internal clearance of radial bearings gradually increases in the following order:

C1, C2, Normal (CN), C3, C4, C5

When to use a larger than normal clearance (C3, C4, C5)
  • To tolerate mounting errors, such as large shaft deflection
  • For high inner ring temperatures, such as when steam passes through a hollow shaft
  • When using a higher interference for heavy or impact loads
  • To account for the increase in inner ring interference at high speeds
  • When both the inner and outer ring have a tight fit
Graph of tolerance ranges for different levels of internal clearance for the same bearing (6210).
When to use a smaller than normal clearance (C2):
  • To drastically reduce sound and vibration during rotation
  • When both the inner and outer rings have a loose fit
  • When clearance will be adjusted after assembly to reduce shaft runout or similar.

Internal Clearance Codes

 

Bearing Type

Clearance

Low

→

(Normal)

→

High

Radial bearings

C1

C2

(CN)

C3

C4

C5

Non-interchangeable*
cylindrical roller bearings

CC1

CC2

CC

CC3

CC4

CC5

Small/miniature ball bearings

MC1

MC2

MC3

MC4

MC5

MC6

Deep groove ball bearings
for electric motors

--

--

CM

--

--

--

Cylindrical roller bearings
for electric motors

--

CT/CM
(interchangeable/non-interchangeable*)

--

--

*Inner and outer rings with non-interchangeable clearances are not compatible with each other due to small range sizes.

In deep groove ball bearings, cylindrical roller bearings, and spherical roller bearings, "E" is sometimes added to the clearance code.
This is an NSK-exclusive code for noise and vibration specifications.

Example designations with the basic designation, internal clearance, cage, and noise/vibration codes defined. C4 and C3 are internal clearance codes.