Success Story
Industry: Railways
Application: Underground Train
Cost Savings: $149,998
Introduction
An overhaul and maintenance company for underground trains in the UK had a requirement to reduce tractor motor bearing service costs by increasing the time between overhauls while still maintaining reliability. NSK Engineers reviewed the greasing procedures during initial build. Improvements were proposed, accepted and documented. In addition, NSK performed a Condition Analysis of bearings that had completed 6 years of service. Using this information combined with NSK bearing lifetime analysis techniques, the overhaul period was increased from 4.5 years to 5.5 years, which aligned more with other components on the train.
- Underground Train
- AIP - Added Value Programme
Key Facts
- Railway industry
- Traction Motor bearings
- 140 machines
- Customer required to reduce service costs by increasing the overhaul time period to align with other train components
- NSK solution: Performing a Bearing Condition Analysis after 6 years of service and reviewing the customer's greasing procedures at initial build and maintenance
- This Engineering Support allowed the bearing overhaul period to be increased from 4.5 to 5.5 years
- Reduced service and maintenance resulted in a significant cost saving
Value Proposals
- Customer requirement to extend major overhaul intervals of traction motor bearings.
- NSK engineers performed on-site examinination of the Traction Motor bearings that had been in service for 6 years for condition, followed by detailed testing at NSK European Technology Centre, to determine remaining bearing life
- Metallurgical examination was performed which included a Bearing Condition Analysis, microstructe check, wear analysis, hardness testing and grease analysis for contamination and water content
- Results concluded that the bearing life could safely be extended to allow major overhaul intervals to be increased
- NSK additionally reviewed customer greasing methods at initial build and at routine maintenance periods, advising changes to the current procedure to help prelong bearing life
Product Features
- NSK analysis uses failed bearings to identify the root cause of problems and makes recommendations for improving both the machine condition and the correct selection of bearings
- Visual and tactile test results
- Early wear indication
- Non destructive tests
- Fully documented report
Cost Saving Breakdown
| Before | Cost p.a. | NSK Solution | Cost p.a. | |
|---|---|---|---|---|
| Engineering Costs: 4.5 years overhaul cycle; 140 machines |
$809, 935 | Engineering Costs: 5.5 years overhaul cycle; 110 machines New procedures extended service life by 1 year and reduced 30 machines per year overhaul |
$659,947 | |
| Total Costs | $809,935 | $659,947 | ||
Reference:SS-E-2022
Share