BEFORE DESIGN FREEZE.

Precision bearings, ball screws and actuator sub-systems —and an NSK application engineer who works the problem with your team — analyze the whole application — and recommends a solution while a change is still a drawing revision.

TALK TO AN ENGINEER

BEFORE DESIGN FREEZE. WHILE THE DESIGN CAN STILL CHANGE.

Precision bearings, ball screws and actuator sub-systems —and an NSK application engineer who works the problem with your team — analyze the whole application — and recommends a solution while a change is still a drawing revision.

TALK TO AN ENGINEER

Not Just a Part Supplier. An Engineering Partner.

Most designs don’t need a custom part. They need an engineer who knows the application well enough to pick the right one.

Usually, What We Already Make

Most problems end here: the right existing product, applied to your condition properly. It is also your fastest and cheapest route — proven, available, second-sourceable.

Adapted Where It Counts

Where an existing design is close, we change what needs changing — clearance, cage, seal, lubricant, material — and leave the rest proven.

A design program, where it is warranted

A small number need one. Whether it's the right thing to do is something we work out with you.




What We Make

Precision Motion Parts, and the Engineering Behind Them.



Bearings

Bearings

From ¼″ × ¼″ thin-section and bores under 10 mm, up to bearings measured in metres.

Ball screw

Ball screws AND LINEAR GUIDES

C0 to C7 accuracy, miniature to ultra-large. Ground in Franklin, Indiana.

Actuators and Sub-Systems

Actuators & sub-systems

Screw, guide and bearings built and tested as one unit. One part number instead of five.



Bearings

Bearings

From ¼″ × ¼″ thin-section and bores under 10 mm, up to bearings measured in meters.

Ball screw

Ball screws AND LINEAR GUIDES

C0 to C7 accuracy, miniature to ultra-large. Ground in Franklin, Indiana.

Actuators and Sub-Systems

Actuators & sub-systems

Screw, guide and bearings built and tested as one unit. One part number instead of five.




Some NSK bearings are specified where nobody gets a second attempt.

Vacuum

Where conventional lubrication stops working.

Cryogenic

And at the other extreme of the range.

No place to stop

An aircraft cannot pull over when a component fails.

Sealed for life

Inside devices nobody will ever open for maintenance.




Why Now

The fix gets expensive on a schedule.

A catalog rating is calculated without your duty cycle, your clearance, your lubricant or the parts around it. If that assumption is wrong, what it costs you depends on when you find out.

▌ Before design freeze — a drawing revision.
▌ After — a change order in production. In service, a recall, end-user downtime, or a field failure.

After-design-freeze-field-failure graph





What you get

Four Things You Leave With.

Send the problem. An engineer reviews it and comes back with something you can act on — so the next design review moves forward instead of waiting.


Video: How our engineers work with customers — “We look at the entire system that the bearing is part of.”

An answer on your part

Does it hold at your loads and duty cycle? Modified rating life to ISO 281 and ISO 16281 — clearance, misalignment, contamination, lubrication.

What we would specify, and why

A recommendation we can stand behind, optimized against cost, mass and reliability. Where more than one route works, you get the options and what each costs. With CAD.

The problem, found early

We model the assembly, not the bearing alone: shaft and housing bending, load distribution, film thickness at your condition.

Something you can actually buy

What works on a prototype has to be manufacturable at your volume, and available when you need it. We answer for that from the start, which is often why the answer is an existing product.







Webinar
Solving Complex Design Challenges for Advanced Technologies

30 minutes, for design engineers. One real requirement, modeled live — and what the model is told about the machine before any number is chosen.

A bearing that fits on paper can still be the wrong one. Bring a question; a simulation engineer answers them at the end.

SPEAKER
CSR, Eddie Ward
NAdeem bhatti

ADVANCED Simulation manager

With 12 years of experience modeling bearing behavior within customer applications, Nadeem brings deep expertise in evaluating stiffness, friction, lubrication performance and bearing life under real-world duty cycles

In this webinar, Nadeem will walk through how NSK works alongside customers during system development, using live simulations to model bearing performance within the actual application. See how this engineering insight can help customers better understand bearing behavior, evaluate design decisions and optimize performance before the system goes into operation.






Where we do this

Pick the One You're Building.

Send the problem. An engineer works it and comes back with something you can act on — so the next design review moves instead of waiting.

Humanoid robotics

Every requirement in the joint fights another one.

Impact loads every step. Stiffness for accuracy against compliance for safety. Lower reduction buys back-drivability, higher buys power density.

What We Size Against

Impact and moment load at the joint

Stiffness and friction across dozens of actuators

Mass and envelope, paid for at every joint above

Whether it can be built at rate

Advanced air mobility

Every gram you save comes back four times.

Less mass needs less lift, less lift needs less power, less power needs less battery — which is less mass again. A milligram of drag in a propulsion bearing is not a component number, it is range. And none of it counts unless the part holds for the whole certified life, because an aircraft cannot pull over.

What We Size Against

Friction and heat in propulsion motors running at extreme speed

Rotor assemblies holding precision and durability over millions of cycles

Tilt mechanisms that must behave the same on the last transition as the first

Certification requirements, which are different on every platform

Space

Some parts only get one chance to work.

A reaction wheel, a deployment hinge that operates once, a cryogenic pump. Nobody services any of them. And some of these conditions cannot be fully reproduced in a lab, which means part of the answer is experience rather than a test result.

What We Size Against

Vacuum, where conventional lubrication stops working

Temperature from extreme heat down to cryogenic

Mechanisms that actuate once, and must

Friction and precision holding across years of operation

Medical devices

It has to hold precision for the life of the device.

A surgical arm, an imaging gantry, a liquid handler. The motion has to stay accurate across the full duty cycle, survive an environment nobody is going to service, and be defensible in a design review.

What We Size Against

Repeatability at the end effector under real load

Smooth, quiet, backlash-free motion of heavy masses

High cycle counts, unattended and maintenance-free

An accuracy grade you can defend, not just quote

Every requirement in the joint fights another one.

Impact loads every step. Stiffness for accuracy against compliance for safety. Lower reduction buys back-drivability, higher buys power density.

What We Size Against

Impact and moment load at the joint

Stiffness and friction across dozens of actuators

Mass and envelope, paid for at every joint above

Whether it can be built at rate

Humanoid robotics

Every gram you save comes back four times.

Less mass needs less lift, less lift needs less power, less power needs less battery — which is less mass again. A milligram of drag in a propulsion bearing is not a component number, it is range. And none of it counts unless the part holds for the whole certified life, because an aircraft cannot pull over.

What We Size Against

Friction and heat in propulsion motors running at extreme speed

Rotor assemblies holding precision and durability over millions of cycles

Tilt mechanisms that must behave the same on the last transition as the first

Certification requirements, which are different on every platform

Advanced air mobility

Some parts only get one chance to work.

A reaction wheel, a deployment hinge that operates once, a cryogenic pump. Nobody services any of them. And some of these conditions cannot be fully reproduced in a lab, which means part of the answer is experience rather than a test result.

What We Size Against

Vacuum, where conventional lubrication stops working

Temperature from extreme heat down to cryogenic

Mechanisms that actuate once, and must

Friction and precision holding across years of operation

Space

It has to hold precision for the life of the device.

A surgical arm, an imaging gantry, a liquid handler. The motion has to stay accurate across the full duty cycle, survive an environment nobody is going to service, and be defensible in a design review.

What We Size Against

Repeatability at the end effector under real load

Smooth, quiet, backlash-free motion of heavy masses

High cycle counts, unattended and maintenance-free

An accuracy grade you can defend, not just quote

Medical devices







test hero

Worked example · robotic joint actuator

The bearing was right. The grease wasn't.

A customer specified a bearing for a robotic joint actuator, and the datasheet confirmed the selection was correct. We modeled the joint rather than the bearing on its own — both bearings, shaft and housing bending, load distribution, clearance and lubrication. At the real operating condition the oil film was too thin for the duty cycle. The bearing was not the problem. The grease was.


No new part. The bearing we already made was the right one — the change was the grease, specified while the design was still open.


What Changed

The grease. Not the bearing.

4.7×
the life the catalog rating alone shows
Same bearing, same envelope. With the lubrication specified for the real duty cycle, the part already selected carries it — no step up in size, no premium bearing, no custom lead time.
1.70M cycles
Rating life, load and speed only
8.02M cycles
Rating life, real conditions modelled
κ 2.1
Viscosity ratio at the operating condition. A full oil film needs a ratio between 1 and 4. The grease originally specified sat below that band — the life above is what the same bearing delivers on the grease we recommended.






How It Works.


01
Send the problem

Loads, speed, duty cycle, envelope, environment.

02
An engineer picks it up

A named application engineer picks it up. Before any work starts you agree together what it needs to be — and how long that will take.

03
You get something to act on

Configurations, trade-offs, the calculation behind them, the CAD.

01
Send the problem

Loads, speed, duty cycle, envelope, environment.

02
An engineer picks it up

A named application engineer picks it up. Before any work starts you agree together what it needs to be — and how long that will take.

03
You get something to act on

Configurations, trade-offs, the calculation behind them, the CAD.

01
Send the problem

Loads, speed, duty cycle, envelope, environment.

02
An engineer picks it up

A named application engineer picks it up. Before any work starts you agree together what it needs to be — and how long that will take.

03
You get something to act on

Configurations, trade-offs, the calculation behind them, the CAD.

01
Send the problem

Loads, speed, duty cycle, envelope, environment.

02
An engineer picks it up

A named application engineer picks it up. Before any work starts you agree together what it needs to be — and how long that will take.

03
You get something to act on

Configurations, trade-offs, the calculation behind them, the CAD.

01
Send the problem

Loads, speed, duty cycle, envelope, and environment.

02
An engineer picks it up

A solution engineer picks it up. Before any work starts you agree together what it needs to be — and how long that will take.

03
You get something to act on

Configurations, trade-offs, the calculation behind them, the CAD.





Support doesn't stop at drawings
And after design freeze

The support doesn't stop at the drawing.

Longer life when conditions aren't ideal

Most bearings don't fail from load. They fail because the lubricant picks up contamination, or the oil film runs thin and the surfaces touch.

We make bearing steels developed for exactly those conditions — Hi-TF and Super-TF — so life holds up when the machine doesn't run the way the calculation assumed.

When something fails, you find out why

Send us the part. The marks on a raceway say whether it was contamination, misalignment, electrical current or lubrication.

Our lab in Ann Arbor reads them and gives you the cause — so the fix is permanent, not another part that fails the same way.





Tell us what the machine has to do.

A simulation engineer reviews it and comes back with what the work involves. If a standard product solves it, we'll tell you that too — and if it isn't a bearing problem at all, we'll say so.