NSK Global
Corporate Profile

You are here: Home >> Company >> Press Lounge >> Press Releases >> NSK Develops a Guide-Dog Style Robot

Press Releases

October 27, 2011
NSK Ltd.
Public Relations Department

NSK Develops a Guide-Dog Style Robot

Autonomous External Recognition and Staircase Guidance Made Possible

Guide-Dog Style RobotTokyo, Japan, October 25, 2011 – NSK Ltd. (NSK; Headquarters: Tokyo, Japan; President and CEO: Norio Otsuka) today announced that it has developed a four-legged, wheeled robot that utilizes a newly developed external recognition technology and guidance function to detect the position of stairs, autonomously recognize the shape of the stairs and then guide the user up and down staircases.

he robot developed by NSK is a four legged, wheeled robot equipped with drive wheels on each of its legs and highly capable of maneuvering over flat and stepped terrain. It is also capable of autonomously recognizing stairs through the use of independent processing of external information detected through image and distance sensors, and then guiding the user up and down staircases. This technology resulted from the development of technology aimed at achieving an autonomous robot capable of assisting human eyesight. This technology has potential application as an alternative to wheelchairs, guide dogs and service dogs. NSK will exhibit this product at Tokyo Big Sight (located in the Koto Ward of Tokyo) from Wednesday, November 9 to Saturday, November 12 at iREX 2011 (International Robot Exhibition). Visitors to the NSK booth will have the opportunity to see a demo and gain insight into the expanding needs of the market. NSK will be performing on-site verification in the actual market in order to confirm the practical use and safety of this product in the real world.

Product features

Guide-Dog Style Robot
New algorithm for external recognition
The robot converts information gained from the distance image sensor into 3D shape, position and attitude information so that it can recognize the width and number of stairs.*1 Conventionally this was a very difficult challenge, but with this new algorithm the robot can recognize stairs while in motion for a safe and stable ascent and descent of staircases.

*1 The fundamental portion of this algorithm is the result of joint research with Chisato Kanamori, Associate Professor at the University of Electro-Communications.

Easy to use guidance feature
Through the use of a length- and angle-adjustable grip as an interface between the robot and the user, the robot is capable of providing stable guidance, even when descending a staircase. The robot is capable of moving at a speed almost as fast as human walking speed, bringing it closer to practical application.
Safety when ascending and descending staircases
The robot is capable of securely coming to a stop when its feet land as it is ascending and descending a staircase. It is equipped with a sensor*2 that limits contact with uneven terrain so as to ensure stable movement and safe guidance for the user.

*2 This sensor is the result of joint research with Makoto Shimojo, Professor at the University of Electro-Communications.

To date NSK's involvement in robotics has been focused on the supply of such products as bearings, NSK linear guides™ and ball screws. In 2007, NSK integrated advanced mechatronic sensor technology with the machine fundamental and component technology NSK had cultivated over the years to develop a robot guide dog capable of autonomous recognition of stairs and the ability to ascend and descend staircases. In this latest version of its robot guide dog, NSK has improved the external recognition, movement and drive functionality and performance, and has added guidance capability.

Through the development of robots designed for human-assistance, NSK will continue working to identify underlying issues in this field, engaging its four core technologies – tribology, materials, analysis and mechatronics – to create robotic solutions to real human needs.

Human Interface

Movable harness

Possible to grip the grip without being swayed by the attitude of the robot

Movable harness

Safety Design

Stable Walking Attitude

The use of two wheels per leg makes it possible for the robot to maintain a stable attitude while ascending and descending stairs.

  • The offset of the wheels is what creates a greater margin of stability
  • The wheels are always oriented in the direction of travel, thus enabling high speed movement using the wheel drive even while ascending and descending stairs.

Conventional robot and New robot

Collision Avoidance for the Legs

Collision Avoidance for the Legs

An array of proximity sensors are positioned on the legs* to confirm contact with the legs and avoid contact with uneven terrain.

* The proximity sensor array was developed as a result of joint research with Professor Makoto Shimojo of the University of Electro-Communications

External Recognition

Recognizing Stairs

Staircase used for measurement

Staircase used for measurement

Continuous extraction of level surfaces

Continuous extraction of level surfaces

The robot extracts level surfaces from the distance information and then reconstructs stair information using an evaluation of the continuous stair surface. In this way the robot can recognize previously unknown stairs, whether ascending or descending.

The robot extracts level surfaces from the distance informatio

Related Information

Latest News

  • Products
    You can find extensive information on our high-quality products, such as bearings, automotive products, and precision machine components.
  • Industries
    As a solution provider, NSK has helped customers in various industries. Here, you can find valuable information to enhance your business performance.
  • Contact Us
    NSK provides our services throughout our global network. For more information, please contact your nearest NSK office.

Go to Top

Copyright (C) NSK Ltd. All Rights Reserved